Hevi-Rail: The Heavy Duty Roller Bearing
Hevi-Rail® is a heavy-duty linear bearing system that is cost effective for medium to low precision applications. The system is easy to mount, align, and use. Hevi-Rail® bearings offer high radial and axial load capacities to ensure a long and productive life under continuous use. This original heavy-duty roller bearing system has repeatedly proven itself in tough environments such as foundries, construction sites, drilling applications, and heavy duty lifting. Businesses have come to rely on Hevi-Rail® guide systems to deliver consistency and overall satisfaction.
Hevi-Rail® is composed of hardened steel, allowing it to excel in the harshest environments. The rails and bearings are designed to evenly disperse load and forces, allowing it to handle up to 60 tons! The result is a combined system that has become the go-to linear motion solution for the most demanding of applications.
Shop our collection of Hevi-Rail® bearing systems today.
Hevi-Rail®: A Radial and Axial Bearing
Hevi-Rail® bearings are designed to handle very high axial and radial loads. This means that Hevi-Rail® bearings can support forces acting perpendicular to the shaft (radial loads) and forces acting in parallel to the shaft (axial loads). This makes Hevi-Rail® systems ideal for a wide-range of high load and telescoping applications.
Load Calculation for Radial and Axial Bearings:
Adjusting Axial Bearings:
- Remove front screws
- Rotate axial bearing shaft (see diagram below)
- Check dimension A (repeat step 2, if needed)
- Re-install front screws
- Recommend use of a breakable Loctite®
Radial & Axial Bearing Applications
Hevi-Rail offers extreme radial load capacities up to 6-1/2 tons per bearing and industrial strength handling applications. This makes the Hevi-Rail guide system a perfect solution for custom lift units and trucks, and heavy load applications in the aerospace, paper, steel, and coil industries. This also allows Hevi-Rail systems to succeed where other linear motion solutions have failed.
One example of the competitor’s linear motion failure deals with a foundry casting tipper. The problem was in the transportation of castings that weighed several tons. Previously, no linear motion system could handle the weight, and would fail after a couple months of operation. This left the foundry with increased production costs and wasted time. To solve the problem, PBC Linear introduced them to their Hevi-Rail system. The Hevi-Rail bearings have been running without failure for well over two years.
The list below offers a more examples of Hevi-Rail applications.
- Material Handling: Other linear guide products rely on precise parallel alignment to reliably handle linear motion tasks such as material handling, lifting and adjustment. They require the installer to conduct a thorough and painstaking checking and re-checking of the monorails to ensure maximum parallelism, resulting in a very costly process. The linear guides also need to be preloaded beforehand for assured system rigidity. In these competitor’s scenarios, when dealing with large loads the preload causes fretting and catastrophic failure in ball-type linear guides and complete stalling in plain bearing products due to exceeding moment load. Hevi-Rail avoids these issues with its unique combined bearing design which allows the bearings to float within the rail, thereby eliminating the need for precise alignment and effectively reducing installation time.
- Telescopic Applications: For high load telescopic handling, Hevi-Rail can support cantilevered loads up to 700 lbs. (318 Kg) extending out 90’’ (2.3 meters). An example of a PBC Linear collaboration with a customer was a design for a new racking system for shipping containers. Previously, the containers were simply filled and shipped, leaving the materials loose inside and able to shift around in transit. PBC Linear worked alongside their design team to create a racking system that could be extended or retracted for easy loading and unloading. This solution required Hevi-Rail combined bearings to handle the extended load and ultimately operate under extremely low maintenance.
- Lift Units: The case-hardened steel design and proven track record of Hevi-Rail bearings have also made it a cost effective and reliable alternative to lift unit tasks. From standard forklifts to custom design systems, Hevi-Rail reduces cost by simplifying assembly and installation. The bearings also thrive in dirty environments and easily roll over dirt, dust and other particulate that would stall ball-type linear guide products. Designed to provide even disbursement of forces throughout the bearing, Hevi-Rail is able to handle radial and axial loads up to 60 tons! Hevi-Rail also requires very little precision due to the floating bearing design. This allows the installer to save time and money, making Hevi-Rail the low cost, long-lasting solution for any heavy industrial linear motion task.
Discover your ideal linear motion solution: